Other Parts Discussed in Thread: DRV8329
Tool/software:
Hello, I would like to ask a technical question regarding the MCF8329A-Q1.
1. Current sensing
I’d like to inquire about the worst‐case error of the current sensor embedded in the gate driver.
In particular, could you please provide information on any factors that may contribute to error, such as gain error, offset, VREF tolerance, ADC conversion error, etc.?
Usage Conditions:
-
Gain: ×20
-
Temperature range: –40 °C to +125 °C
-
Shunt resistor: 2 mΩ, tolerance ±1 %
2. loss of phase
I would like to use the loss‐of‐phase feature for phase‐open diagnosis. Is it necessary to run the motor in order to perform this diagnosis?
Could you please explain how this feature works?
Thank you for your assistance.