This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCT8329A: Motor is blocked

Part Number: MCT8329A

Tool/software:

Hi ti team,

The application test issues regarding MCT8329A1IREER are as follows?

When the motor is blocked, a fault code will be stored in the fault register of the chip. Under normal circumstances, by inputting a command to clear the fault, the fault code in the register can be erased and the motor can operate normally. However, now the fault code cannot be cleared using the TI erasure method, and the motor cannot work properly. The current triggered fault code is loss of sync.