This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8705-Q1: Technical enquiries regarding SPI on DRV8705-Q1

Part Number: DRV8705-Q1

Tool/software:

Hello, Motor driver team,

Customer is working on SPI Driver for SPI communication with MCU on DRV8705-Q1.
And Customer got the result value by writing it on STAT_2 for review during work, but SCLK_FLT was set to 1.

It seems that there was no problem with the specific as shown in the picture below (Figure 6-1. SPI Timing Diagram.),
Customer would like to ask if there are any other conditions for SCLK_FLT to occur. (Please refer to the customer's Analyzer measurement image.)

Figure 6-1. SPI Timing Diagram

customer's Analyzer measurement image