Tool/software:
Hello,
My customer has some questions for OLD function of DRV8910-Q1.
Low-current acitve OLD looks like supporting only L outpt. Can't it be used for H output?
The active OLD current is defined as 2~18mA(TYP 9mA). This is too big for their application.
Is there any way to reduce it?
2mA MAX of Low currect active OLD is good, but it looks like not supporting H output.
They need to support both H and L outputs
And doesn't DRV8908 support passive OLD?
Regards,
Oba