Tool/software:
As we know the MCT8329A uses a sensor less motor control algorithm to drive a motor. In this case it will use back-emf the check the motor speed and control the speed according the input control in a closed loop approach.
My query is since there is no ADC input pin then which pin is used to measure the back-emf (feedback of motor speed/position).