Part Number: LM25148
Tool/software:
Hi
Could you help check the below LM25148 schematic and any need to adjust
1. LM25148
Intended put out 11V at 16A, with wide range of 9V-36V. Attached is also the excel calculation used to design at Vin (nominal ):12V
May I know if the device can still work if the input goes lower range 12V-9V, perhaps with some losses (eg: CCM, output voltage drop)?
Does AGND connection to PGND need shortpad/net bridge, or just directly connect will do?

Your help is greatly appreciated. Thank you.