This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8353F: DRV8353F register setting review

Part Number: DRV8353F

Tool/software:

Hi, we have designed DRV8353FS drive and 3x half bridge circuitry (schematics as attachement spreadsheet and MOSFEt datasheet as below). Please help review what we setup on regiesters are proper or not. Anything inappropriate please kindly let me know. Thanks.

Note: For target output rise time/fall time, we are not sure how to define them (see DRV8353F: How to determine 'Target output rise time' and 'Target output fall time' - Motor drivers forum - Motor drivers - TI E2E support forums). So they are temporarily same as datasheet.

MOSFET datasheet link: www.mccsemi.com/.../drv8353f-config-for-review.xlsx:320:240]

  • Hello,

    Yes, the rise and fall time will be most affected by the IDRIVE settings. 

    The links you shared are not working, so I cannot see the registers or mosfet you have selected.

    But, it is likely that you will not need the max IDRIVE setting that 8353 is default with. I would recommend starting with a lower setting (300mA source/ 600mA sink), and see if that is working for you first.

    Too high of an idrive setting will cause problems in your system.

    Thank you,

    Joseph