Tool/software:
Ibinu,
It's been a while and the drv3946 is working very well for us.
However! (There's always a however, isn't there? :) We are seeing some strange behavior that we are at a loss to understand.
The behavior is a bit of a story, so please bear with me on this.
We are running valves that operate at 24 volts. What we noticed is that when the valves are placed close to each other, and one of the valves is turned on or off, the adjacent valves respond with an "Open/short" error. THis turned out to be due to the EMI field generated by the coil being controlled would generate a spike on the adjacent coils due to the growing/collapsing magnetic field of the operated coil causing the adjacent coils to generate a voltage that the drv3946 interpretted as an open or short condition and would then disable the valves. The fix was to use EMI shielding around the coils. This worked to mitigate this particular error.
What we are seeing now, though, is a single valve that is NOT in proximity to any other valves, nor is the wire connecting it running near any of the other valves, yet, the valve will generate the open/short condition error on it's own when the valve is activated for about 12 minutes (This allows it to heat up) and then when it's deactivated, it generates the open/short condition error.
I can imagine a ton of scenarios where this might be true, marginal connections, something wrong with how the valve was made etc etc etc.. But it gets.. weird. I can drive an identical valve and cycle it every one second.. after 40,000+ iterations of this test, the error never shows up. The same is true with the failing valve! I can cycle it continuously for extended periods of time with no error. However, if I start with it as a cold valve (Like, physically cold not been run for a while) and energize it for 12 minutes, then turn it off, it throws this error. Once the error has occued, I can clear the error and then cycle the valve continuously every few seconds and it does not throw this error.
What I am looking for from you is ANY list of ideas of things I can look at either on the drv3946, or in regards to electrical measurements I can make on the valve itself or in conjunction with being operated by the drv3946 to determine exactly what is going wrong with this valve.
I look forward to your thoughts on this matter.
Thanks
Rick