Tool/software:
Hello,
My customer is interested in DRV11873. Would you please give me your comments for the followings?
Questions
1. Can DRV11873 control the rotation speed without correct PWM input like no PWM input or 0Hz(DC) input? I see some issues at no PWM input from the past E2E posts like the following. I'd like to know the root cause, but the thread doesn't show that.
DRV11873: DRV11873 related issues - Motor drivers forum - Motor drivers - TI E2E support forums
2. This question is related to the above one, but what would happen if there is no PWM input or lower than 7kHz PWM frequency? Please tell me if it depends on the pin conditions.
Best Regards,
Yoshikazu Kawasaki