Other Parts Discussed in Thread: DRV10975, DRV10983, MOTORSTUDIO, MCF8315C, , DRV10975EVM
Tool/software:
Hello,
I have been attempting to tune several BLDC motors with the DRV10983 and DRV10975 evaluation modules. The motors I am working with are within the specifications for both DRV10975 and DRV10983, however, they produce very low back-emf. I do not currently have the exact back-emf motor constant, Kt, since I do not have datasheets for the motors, but I know from testing that it is very low and I expect it to be on the low end of the acceptable range for these EVMs. When I follow the tuning guide I am able to get them spinning in open-loop, but see very poor performance transitioning to closed-loop control, after which they immediately lock up. Additionally, the RPMs reported in the GUI are much higher than the actual RPM, which is typically the error I get that resulted in the automatic shutdown or lockup. For example, the motor will be spinning around 2000 rpm according to a tachometer, but the GUI will report values in the range of 18,000-20,000 rpm. Is there any way you can help me isolate the issue here? I have been assuming it is due to the low back-emf produced by these motors, but there could be something else I am missing. For reference, these motors are able to spin up to 20,000 RPM or greater using commercially available drone ESCs, but I am hoping to get better performance and reliability out of the TI motor drivers.
Thank you!