This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8844: Unknown behaviors for FMECA

Part Number: DRV8844


Tool/software:

Dear all,

I am doing FMECA (Failure mode, effects, and criticality analysis) on an electronic board that includes the DRV8844.

I am having difficulty deriving possible behaviors of the component in 4 specific cases. Could you help me?

The cases are:
- the capacitor between VCP and VM is open (interrupted)
- the capacitor between VCP and VM is short-circuited
- the capacitor between CP1 and CP2 is open (interrupted)
- the capacitor between CP1 and CP2 is short-circuited

What should I expect on the OUTs? What should I expect, in general, from the device? The datasheet does not report indicative data to deduce its operation, without the need to perform a targeted failure test.

  • Hi Giovanni, 

    Thank you for your question. 

    Following are the assumptions of use and the device configuration assumed for the pins

    the capacitor between VCP and VM is open (interrupted)

    The charge pump is used provide a gate drive voltage higher than the VM power supply  to fully enhance the high-side FETs. If VCP is open, the VCP stays at 0V or undefined and the High side MOSFET can not go high. 

    the capacitor between VCP and VM is short-circuited

    In this case since the gate drive voltage is not higher than VM power supply, the High side MOSFET cannot go high. 

    the capacitor between CP1 and CP2 is open (interrupted)

    the capacitor between CP1 and CP2 is short-circuite

    The capacitor between CPH and CPL is essential for generating a boosted voltage on VCP. Shorting / opening these pins is like removing the energy storage element of the pump.
     Without proper switching across a capacitor, the charge pump cannot step up the voltage. VCP will remain low and insufficient to turn on high-side MOSFETs and The outputs (OUTx) cannot drive high.

    Please let me know if you have any more questions. 

    Best regards, 

    Mojtaba,

  • Hi Mojtaba,

    Thanks for the point-by-point reply. Everything reported seems reasonable to me.

    Sincerely,
    Giovanni

  • Hi Giovanni, 

    Thank you! Please close this thread if this issue is resolved. 

    Best regards

    Mojtaba.