This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV10964EVM: Unable to drive high speed drone motor

Part Number: DRV10964EVM
Other Parts Discussed in Thread: DRV10964, MCT8316A, MCF8315C, DRV8311HEVM, DRV8311

Tool/software:

I’m trying to use the evaluation module to drive a VCI 22000 KV drone motor. Since its maximum speed exceeds 900 Hz, I set the Config pin to 4.85V and supplied 3.7V to power the motor. However, I’m not seeing any response from the controller or the motor. I also tried a lower 11000 KV drone motor, but there was still no reaction. Interestingly, I was able to successfully run a Maxon 371122 motor (no-load speed: 15,600 RPM) even without using the Config pin. Do you have any suggestions on what might be causing this issue? Thank you!