Tool/software:
Hi,
I have a lens module in which the lens' aperture is controlled via a DC-Iris motor (2 Iris Blades mechanism galvanometer drive). I wish to control the lens to fully open, partially open i.e. (25%,50%,75%) and fully close. Could you please recommend a suitable motor driver that can accomplish these functions?
My DC-Iris has 4 wires: 1. Driving+ 2. Driving - 3.Stopping+ 4. Stopping-. I have a Panasonic AN41908A demo-kit that can perform above function through the Iris Drive internal module but I want to explore other alternative parts because there is lack of documentation from Panasonic explaining how to configure the IC to properly drive the driving and stopping coil of DC-Iris. I looking at the datasheet of TI DRV8837 but there is only two wires available to connect to the motor (my DC-Iris has 4 wires)
Thank you