Other Parts Discussed in Thread: DRV8876
Tool/software:
Hello Team,
I'm designing a motor drive for DC motor of power rating 12W and the input is a 12V system. I considered DRV8876 as the driver IC and it I'm following the reference given in the datasheet. Apart from the inbuild protection technique, I would like to introduce some protection technics in the load side (using some capacitor, diode). Unfortunately, my driver circuit will be away from the motor and the connection is established using long wire. Is there any recommended technic for the load protection? Since the due to the long wire (1m), there will be some effects due the wire transient.
Thank you.
Regards,
Jishnu