Part Number: DRV8220
Tool/software:
using the DRV8220 in PH/EN Mode with low duty cycle will go to auto sleep in "normal operation"
I drive a small DC Motor with direction contol connected to PH and a 8bit PWM to the EN Pin of the driver. Mode and Sleep is µC controlled by constant set to high during initialisation.
typical PWM frequence is 10kHz. If the the high periode is less than 4.5µs the driver go to sleep, if duty is increased to >16µs the driver will restart. frequency on the PWM = EN Pin is constantly running.
If i change to 20 or 40Khz the problem increases as i can only use the dutycycle >80%.
This was not expacted after reading the datsheet. What is the minimum PWM Pulse-width the device can handle?

EN-Signal PWM input (yellow) and OUT1(green) while changeing the duty cycle