Tool/software:
Hi,
The requirement is to drive two or three DC motors using a single DRV8235 motor driver, where the motor driver is controlled by an MCU.
So, I need some ideas to switch between the motors using a single driver. Given that driver can drive only one motor at a time.
The motor needs 5V of VM to operate with a minimum current requirement of 300mA.
It would be very helpful if I get information regarding this.
Thank you.