Tool/software:
Hello expert
An issue occur about the SPI Error Indicators and the LSD initiation failed.
I am doubting that the nFAULT/NAD pin Pull-up Resistor exceed the limit range.
One LSD's NAD pin pull-up Resister is 27K, the measured value is 26.6K, I am not sure if it's exceed the limit.
The recommended accuracy of resister in datasheet is 1% as below.
BR
LinSong