Tool/software:
I plan on setting the voltage level of the VDSLVL pin with a pwm signal so that it is adjustable through software. If software sets it too low, will there no longer be an overcurrent level where the DRV8162 device no longer has shootthrough protection for the switching mosfets?
Is there a low level voltage level for VDSLVL where it finally turns off the DRV8162, or can the VDSLVL be set all the way to zero volts to disable any overcurrent threshold?