This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCF8316A: About BRAKE's pull low location.

Part Number: MCF8316A

Tool/software:

Hi team,

I have 2 question with MCF8316A

1. I suggest the Brake pin connect AGND via 10K to customer, but the datasheet indicates connecting PGND via 10K if do not used. What is different?

2. If the power buck in the EVM is in resistor mode, the resistor size is 2512. If I don't have a load on this power buck, can I use a 0603 resistor?