This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2510-Q1: Bandwidth limits

Part Number: DRV2510-Q1

Tool/software:

Hello Team, following question missing in our datasheet:

---

Usually, we have an bandwidth of DC up to ~ 1-2 kHz.

Now, within a new design we want to use the DRV for a wider bandwidth signal.

The desired signal has bands up to 12kHz ~ 16 kHz.

 

Now: I can’t find any characteristics / measurement reports for the H-Bridge limits in terms of short timing (Ris/Fall times) / or frequency bandwidth inside the Datasheet.

 

Can you support with more information’s on that for us?

Many Thanks

Josef

  • Hi Josef,

    Sorry for the lack of information here. Since this part was made for solenoid drivers (typically low frequency), there was no need to list a bandwidth limitation or slew rate. That being said, you can get 20kHz bandwidth out of this device. Will this be sufficient for you to move forward?