This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8412 EVM kit

Other Parts Discussed in Thread: DRV8412, CONTROLSUITE

I have just obtained the DRV8412 motor contol kit as the example applications for stepper motor control closely match my end application.

I was hoping to use the source for this demo as a starting point and build my appliaction around this.

However, the soure for the project that comes flashed in the kit doesn't seem to be included anywhere in ControlSuite.  Neither is the source for editing for the GUI front end if you have the Crosshairs suite.

There is just a cut down example project for CCS for driving either steppers or brushless DC.

According to the quick start guide they should be here:

C2000 source code for the GUI project can be found at

controlSUITE\development_kits \DRV8412-EVM\GUI_projec

Crosshairs Embedded GUI .exe and project files can be found at

controlSUITE\development_kits \DRV8412-EVM\~GUI

 

Can anyone help please? 

Thanks

James