Tool/software:
Dear Support Team,
Under which condition is it possible that the driver, without any configuration (thus should be running with the default config), passes the VM supply voltage directly to the motors?
Every time I do not send a config to the motors and only enable the driver, I see a current draw of more than 1A from my supply, although the motor is rated at only 180mA. The motor heats up very quickly, as if the driver were practically connecting VM directly to the motor.
My Vref is 1.1V, so the maximum current should actually be:
1.1*100%/2.2 A= 0.5A
When I send my normal configuration with 50% TRQ_DAC, everything works fine again.
Vm is 28V. Motor phase resistance = 16Ohm.
Thank you very much for your support.
Best regards,
Lyto