This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCF8329A-Q1: Operation when PWM duty is 100%

Part Number: MCF8329A-Q1

Tool/software:

Dear TI experts,

My customer tests MCF8329A-Q1 in their own PCB.

In that test they need to operate the motor with 100% maximum speed if PWM duty cycle is 100%.

-> If the customer set DUTY_OFF2 register as 255 and set PWM duty cycle as 100%, Can the motor operate with maximum 100% speed?

or it can be operate abnormal due to DUTY_OFF2 register(255)?

Please check this issue. Thanks,

Best regards,

Chase