Other Parts Discussed in Thread: LMG3100R044, , TIDA-010276
Tool/software:
Hello,
I am a beginner engineer working on a motor drive design and would appreciate your guidance on component selection and specifications.
My Requirements:
- Input voltage: 48V DC
- Continuous operation: 30A RMS
- Peak operation: ~80Apeak for approximately 3 seconds
- Application: Motor drive system
Questions:
- I am considering between LMG3100R017 (126A rating) and LMG3100R044 (46A rating). Which would be more suitable for my application requirements?
- I plan to base my design on the TIDA-010276 reference design. Is this reference design appropriate for my specifications?
- Current Rating Clarification: Regarding the LMG3100R017's 126A specification - can you confirm this is the RMS current rating? I want to ensure I understand the datasheet correctly for proper thermal and electrical design considerations.
Thank you for your time and assistance.
Best regards,
Han.