Other Parts Discussed in Thread: DRV8412, DRV8840
Hi all
I'd like to know why instead of having a constant voltage at the DRV8412 output am I getting something like sawtooth voltage? and because of this the motor starts to spin but immediately the voltage starts to decrease and so the motor speed until it reaches what it seems to be a low-level-trigger and then jumps immediately to the supply voltage and the cycle starts again.
The motor power supply is 12vdc, I´m using mode 4 (as explained in datasheet p.14) because I have a simple DC motor in outputs AB, so, when I put a 0 in the line "RESET AB" then the output jumps to 12 volts and the motor start to spin, immediately the voltage starts to decrease aprox 1.2v/sec (no charge at the motor) until it reaches 2.6V aprox and then it jumps to 12 V again but immediately the voltage starts to decrease and the cycle repeats.
If I apply some charge the voltage decreases faster to the same 2.6v aprox. but it does the same pulsing response. Any Ideas?
Thank you for the answers!! Regards