This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8353: Split ground design with multiple gate drivers

Part Number: DRV8353


Tool/software:

Hello,

I would like some advice on how one should split the power and digital ground in a multi-channel motor driver design.

For a single channel driver, the recommendation is to put a ground tie near the DRV8353. But for multiple of these gate drivers, where would the star point go?

Since I intend for each channel to operate high power motors I am concerned that there will be a shift in the ground potential at maximum load. And that it may interfere with the current sense readings if the digital and power grounds are changing slightly relative to each other.

I am also wary of stitching the ground planes with net ties at each channel's gate driver as it may provide unintended high current return paths through the digital domain.

Please advise what layout methodology I should use here.

Thanks,

K

  • Hi K,

    Like you mentioned the main point of concern when considering the net tie placement is to avoid the noisy high current paths going through/over the digital planes/traces. You can use multiple net ties, as this may make it easier to create smaller return loops to avoid large noisy loops.

    Either way should work, but it is ultimately dependent on your specific layout in order to minimize the interference from PGND current.

    Thank you,

    Joseph