Other Parts Discussed in Thread: DRV8300
Tool/software:
Hello:
Design Requirements:
1. Input Power: 12S Lithium Battery, approximately 40V-51V
2. Driving a BLDC Motor (output continuous current 60A, instantaneous maximum current 100A)
The design circuit is attached. I have the following questions:
1. Can the DRV8300DRGE gate pin drive three MOSFETs (TPH4R50ANH1) simultaneously?
2. Is the damping resistor connected in series with the gate pin still 10 ohms?
3. Is the gate drive voltage still designed to be 10V, or does it need to be increased?
4. Does DT need to be adjusted to drive multiple MOSFETs at once? Are there any recommended values or calculation formulas I can use? Design Requirements:
5. My design circuit diagram is attached. Could you provide some design advice?
Thank you!