Other Parts Discussed in Thread: CSD19536KTT, DRV8161, DRV8162
Tool/software:
Hi,
We are taking DRV8161EVM to production for 2 wheeler electric vehicle application.
We wish to scale the design from 30A to 150A peak currents (for 2 mins) & nominal currents of 50A. The current sense & other updates are completed and functional design is okay.
Present design query is related to thermal design with the above changes:
Following are the queries:
- Let us know if thermal vias used for CSD19536KTT in DRV8161 should be tented or untented. (Some images are attached for reference)
- let us know maximum copper layer thickness we can achieve in this design.
- Let us know recommended spacing between tracks & track width for increasing the Finish Copper layer thickness to 140μ/4 oz & Inner Copper layer thickness to 70 μ/2 oz
Let us also know if there are additional reference design using CSD19536KTT & DRV8161EVM with higher currents that we can refer to.
Have a good day.