Hi,
I am confused about the Power ratings of your DRV8412 motor driver IC . I have used DRV 8412 samples on our new PCB design and would like to know what maximum continuous current it could theoretically withstand before overheating. The data sheet suggests a 6A continuous output current per chip and that in can drive motors up to 50V. This would suggest that using the parallel mode, this driver IC can drive a 300W motor which doesn't make sense. On page 3 of the data sheet under "PACKAGE HEAT DISSIPATION RATINGS" chart it is suggested that the resistance from junction to ambient is 26.1 degrees/watt. Since the DRV8412 is %97 efficient T_junction= 125 = (100-97)/100 x outputpower * 26.1 + 25 => outputpower = 3.83 watt. On the same page (page 3), the "PACKAGE POWER DERATINGS" suggest that the pakage power rating is 5watts at room temperature. So overall I am confused about the power rating of the DRV8412 device. If the recommended data sheet exposed power pad / heat slug area is met what is the power rating of the package? or in other words how many watts can it continuously output? My motors are 6-10 Volts and I'm trying to find out how much continuous current the DRV8412 can withstand.
Thank you for you help,
Darius