Tool/software:
Hello, I would like to drive a BLDC motor with the MCF8329EVM. I don’t want to damage the board. What should I be careful about? For example, in this post it is mentioned that if the deadtime is not set correctly, the MOSFETs could be damaged: https://e2e.ti.com/support/motor-drivers-group/motor-drivers/f/motor-drivers-forum/1514312/mcf8329evm-mcf8329evm . I would like to learn about things like this. Thank you. Some data about my BLDC Motor:
Number of Poles: 8
Phase-to-Phase Resistance: 0.25 ohm
Phase-to-Phase Inductance: 0.13 mH
Back-EMF Constant: 0.023
No-Load Speed: 9853 RPM
Nominal Voltage: 28 V