This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2605L: haptic ic

Part Number: DRV2605L


Tool/software:

Hi 

My customer's application is for a 15.6" monitor related to medical applications. Please recommend a suitable Haptic IC. Currently, the entire display needs to be oscillating.

Thank you.

  • Hi Gareth, 

    I think for a monitor of this size either multiple DRV2605L devices and multiple LRA/ERM haptic motors can be used. multiple Haptic motors can be triggered simultaneously through external hardware trigger.

    the DRV2605L comes with a few benefits. since it has an internal waveform memory with a library of 123 haptic effects it can be very simple to find the effect which meet the requirements

    Alternately a high power driver like DRV2510 can be used. with a much larger single solenoid it can likely create the necessary haptic effect in the display 

    Since DRV25010 is an analog input device you will also need some external DAC to create the waveform. even DRV2605L could be used as the driver for DRV2510. 

    Regards,

    Arthur

  • Hi Arthur

    Thank you for your information.

    How do I synchronize and control multiple DRV2605L? Is there a reference schematic?

  • Yes, We actually have an EVM which can be used to evaluate this use case

    DRV2605LEVM-MD Evaluation board | TI.com