MCF8316C-Q1: Using Two Drivers for Two Stators

Part Number: MCF8316C-Q1

Tool/software:

If I wanted to spin a single rotor using a dual-stator strategy where each stator is run by a MCF8316C or D. I am assuming that by giving the same drive commands they would produce effectively the same force on the rotor and when they speed is high enough both should measure the same BEMF so they would effectively synchronize with any small misalignments not being a problem because each would synchronize itself to the rotor.

Is there any reason this wouldn't work/any ways to improve this approach?