This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8889-Q1EVM: Where do I get firmware for the MSP430Fxxx that's on the DRV8889-Q1EVM?

Expert 2055 points
Part Number: DRV8889-Q1EVM
Other Parts Discussed in Thread: DRV8889-Q1, MSPM0L1306

Tool/software:

The stepper motor driver board has that MSP430F261X-PM64 on it, and it has debug connection. But I cannot locate any links to the firmware project for it in any of the DRV8889-Q1EVM documentation.

(There is an available project with drv8889-q1 firmware/library to use if one users an external MCU such as MSPM0L1306, but that requires to buy external MCU/board).

Could you share please that code for that onboard MCU?