Other Parts Discussed in Thread: DRV8306, CSD, CSD88599Q5DC, , DRV8363, DRV8353, DRV8323
We are currently designing a motor driver brd to control a 36Volt BLDC---The motor only draws 3 to 5 Amps---We are using a DRV8306 to drive the motor CSD88584 FETs---as mentioned we are seeing failures after several weeks of running the motors---We pretty much copied the eval brd design which was optimised for 24VDC operation ---We are susupecting that because we are running the FET near its max VDD(36V) some ringing might be pushing it over its max VDD. So we are going to go to the CSD 88599 FET with a Max Vin of 60Volts . My question is can the ringing on the VM line possibly get into the VM input on the DRV8306 and if so can a RC filter feeding the 8306 be an option . Additionally I noticed in the data sheet for the motor FET a note stating a snubber circuit shoud be use either instead of or additionally to the .01uF bypass caps on all the FET VINs. As mentioned earlier we are suspecting ringing to be the issue in the design.The enginner involved on the project has did some preliminary measuring but has been pulled away so he has not gone thru the brd in detail with a scope to look for ringing . Would appreciate your thoughts ----Thanks, Mike Titta R&D