Part Number: DRV8718-Q1
Dear TI experts,
My customer have a plan to control 1 DC motor using DRV8718-Q1.
For controlling 1 DC motor for both direction, customer need 2 half bridges.
So they want to control 1 more DC motor for only one direction.
- Is there any problem to control 1 DC motor for only one direction using only 1 half bridge of DRV8718-Q1? (In this case 1 half bridge remains as floating.)
- Or, Should I use remained 2 half bridges even I want to control DC motor for only one direction?
- And one more question. Is there any RPM limit if I control DRV8718-Q1 through SPI interface? (i.e. I use DC motor which maximum rpm is 1000, but DRV8718-Q1 can control only up to 800 rpm if I use SPI interface.)
Please check these issues. Thanks.
Best regards,
Chase