Hi,
I've recently gotten back a PCB with a DRV2700 on it and I'm not getting the expected voltage from the boost converter.
The plan is to get ~90V from the BST pin, to do this we figured that powering SW from +12V would make the DRV2700 have an easier time of it. L1 is a Wurth Elektronik's 74438357056 5.6uH WE-MAPI inductor.
As per the datasheet for the DRV2700 the Ilim was set to 2.3A (inductor saturates at 3.9A so we're good) so Rext was chosen to be 6.04k. I'm expecting a duty cycle of 91.1% and switching frequency of around 918kHz as recommended by the datasheet.
However I get a voltage of 10.92V at the BST pin. That suggests to me that the MOSFET is not switching. Do you have any suggestions on what I could try to fix this and get ~90V on the BST pin?
Here's my PCB Layout, this is a 4 layer, 1oz on all layers, 0.8mm thick PCB. The top layer has most of the signals/traces, inner 1 is GND/0V, inner 2 is a continuous +5V power plane and the bottom layer is mostly GND/0V but it has trace for BST back to the feedback resistors R1 & R4 placed next to the FB pin and the input +12V supply.
Thanks!