Part Number: DRV8316-Q1
After the chip restarts, which pin should I check, or is there another way to make sure it’s reset properly?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DRV8316-Q1
After the chip restarts, which pin should I check, or is there another way to make sure it’s reset properly?
Hi Max,
What are you wanting to check? Are you wanting to check when the device is ready after restarting the chip? typically this is 1ms after nsleep =1

Regards,
Yara
Hi Yara:
I wanna check if the chip’s restarted. Like, for a car’s infotainment system, if there’s a boot-up animation when it restarts, or if the version info shows up in the logs, you can tell it’s restarted. So for the chip itself, how do you figure out if it’s been restarted?
Hi Max,
I believe the NPOR bit is latched in the event VM loses power


However if nSLEEP is used to reset the device then there is no indication that the device was reset.
Regards,
Yara