This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8849: LV8044LP replacement

Part Number: DRV8849

Hi Sir,

My customer is looking for a dual stepper motor driver solution to replace the LV8044LP.pdf.
A key requirement for this application is that the motor power supply voltage (VM) must support a minimum of 3.3V.
Please provide your recommendations if there are any suitable ICs for this application.

  • Hi Henry,

    Thanks for your post. See here the list of drivers in our portfolio that could be used to drive stepper motors with minimum of 3.3 V VM supply voltage. All these are dual full-bridges, they can driver one stepper motor or two brushed DC motors. We do not have an exact equivalent of the mentioned LVxx device. The DRV8849 dual-stepper driver requires a minimum 4.5 V for operation.

    Regards, Murugavel