Part Number: DRV8323R
After reading the datasheet and performing some experiments. I am confused about the reference voltage to be used while current calculation.

- I am using Unidirectional current sense application.
- My Vref voltage is 3.3V
- Considering the equation (4) as given in above image and taking Vref = 3.3 V, i am not getting the correct values of current.
- However on changing the Vref to 3V in calculations all the values that I get for current reading are perfectly matching the current consumption.
- I do understand the current consumption graph as given above shows that linearity can only be obtained in range from 3V to to 0.3V, however in the equation it does not state that 0.3 needs to be deducted or not from Vref.
Why is that 0.3 needs to be deducted?
Is that the bias volatge of interanl Op-Amp?
Any help will be appreciated.
Thanks,
Tirthraj