Part Number: DRV8703-Q1
Hello!
I'm having a problem: the chip keeps failing—either immediately or after a while. The chip driver is connected to the motor via MOSFET transistors, but the motor isn't running, so the driver isn't being controlled. The 24V line is protected by a TVS diode. The resistors R1, R7 and R8 then get very hot and fail. The chip itself then shorts out on almost all of its pins. The Mosfets transistors are ok, don't fail. We have two grounds, G and PG, which are shorted at a single point. The chip often fails when connected to a 24V battery. Last time, we powered it from a power supply, and it later simply failed on its own without being used. Help!