Hello-
We have built prototype boards with DRV8825 ICs and have found an issue with noise. The switching frequency should be 30KHz but depending on decay mode and step number, the frequency varies between 12 and 28 kHz. Vref A and B are set at 1.59V and the current sense resistor value is 0.68 ohms.
There are two issues with the low frequency:
1. audible noise
2. high ripple current
The frequency should be relatively constant as the modulator design is fixed frequency, peak current mode. (See data sheet page 9 first sentence.) Is there something malfunctioning causing the frequency to change more than 2:1 depending on the mode and operating current? I also see double pulsing at times.
Schematic is attached. Grounds are connected to internal plane. +24V is supplied from large bank of low ESR caps close on the PCB. I tried eliminating the fuse resistance with no change. Motor winding is 13 ohms, 7mH. What is causing the issue and how can it be remediated? Thanks and Best regards,
-Tim Starr on behalf of SN@NM