This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

drv8825 fault pin

Other Parts Discussed in Thread: DRV8825

the nfault pin of drv8825 is always in low state.... why ?

  • Hi Arun,

    A few things you can check:

    1. It is possible one of the outputs are shorted to the other output (e.g. AOUT1 is shorted to AOUT2, or BOUT1 is shorted to BOUT2), shorted to VM, or shorted to GND. If so, this is will generate an Over Current Protection event and the device will latch on the fault state.

    2. Is VM larger than 8.2V?

    3. Can you check to see if the charge pump VCP pin is larger than VM? It should be at least 10V higher.

    Let us know if any of these recommendations help. Best regards,

    Jose Quinones