Part Number: MCT8316AEVM
Other Parts Discussed in Thread: MCT8316A, MCT8329A, MCF8329HS
I had installed the GUI platform, As mentioned in the Hardware setup "Read All registers" option not there, instead of load register option there, but what register s need to be loaded? Hardware connection gets disconnected. I installed version 1.0


I could able to configure with the latest version. With 20V supply, in analog mode motor is rotating with minimal speed. But in display as attached electrical speed not showing and motor in Idle state is displayed. I had taken pole pair: 7 with mechanical speed: 15000 rpm. The electrical speed obtained is 3000Hz. Abnormal Speed Lockout threshold given is 1250Hz. The maxon motor used: EC-i 608328.
Hi Dinesh,
I am facing issue in the operation of motor. I had shared the screenshot of the motor details and the result of the motor under run mode. I had operated at 28V DC with pole pair: 4 and CBC current limit of 8A with CSA gain 0.15V/A. the tuning parameters provided were A1= 10Hz/sec, A2= 20Hz/sec. Closed loop accel 3V/sec. First cycle frequency 3 Hz. Align time 250msec. Initial max mechanical speed :1000 rpm. But the motor is providing some sound and not rotating.