Part Number: MCF8316D
Other Parts Discussed in Thread: MOTORSTUDIO, MCF8329HS
Hi,
I'm trying to tune a MCF8316D driver with a LS-7060 DC Centrifugal Brushless Air Blower motor. The datasheet is attached.
I'm using motor studio with the MCF8316D dev kit. The dev kit is powered by an external supply running 24V with 5A current limit. The dev kit hardware setup as described in the motor studio hardware setup.
I've tried to use the smart tune, but it can't ever generate the configuration successfully. Here's the parameters I've been using:
Load: Load or No Load
Rated Voltage: 24V
Rated Current: 2-8A
Rated Speed: 1345Hz
Control Mode: Speed mode
The Optional parameters I've tried including them or not, neither successfully generates the config.
Phase Resistance: 0.165 Ohm
Phase Inductance: 0.074 mH
BEMF Constant: Always empty
If I have the current high, the motor doesnt turn on. If i set the current lower (3-4 A) then the motor does turn on during the tune sequence, but cant get past about 60% speed, so the configuration generation fails. The most common error codes I get are HW_LOCK_LIMIT or BEMF_FAULT.
I've also tried the MPET which also always fails.
Any help would be greatly appreciated. Let me know if you need any other information. The motor can spin and can be tuned with lower current and speed but with the datasheet values it doesnt work successfully. Thanks.