Part Number: DRV8870
Dear TI Team,
We are using the DRV8870 device since many years on one of our product.
It's driving a small DC motor.
The DRV8870 is suppyed in 24V, and its commands are in ON/OFF 0_5v signals on its 2 inputs (IN1 and In2) to move the motor in the 2 rotations.
The sense resistor is fixes to 1 ohm, and Vref is 3V, which indicate a current limitation of the devide to about 300mA.
We can observe it with devices which are running, at the beginning of the rotation of the motor, output out1 or out 2 are switch on and off to "regulate " the current to 300mA for about 200msec.
It was well working since many years, but we have now troubles with it, motor doesn't start it rotation.
We have observed that the DRV8870 looks to enter directly in over-current limitation cycles, with 3msec off sequence before restart and switching off again.
We have a batch of boards with this behaviour. During checking, we have noticed that a way to start the rotation is to shunt the sense resistor. But we can't explain this behaviour.
Do you know some modifications on the design of the DRV8870 which could explain this, and which modification would be required ?
Thanks in advance