I want to use drv8432 in my project for controlling brushed dc motor. While making the pcb i didn't find the model of drv8432dkd (36 pin) in any PCB software. In the forum somewhere I found the design files you have given(5811.DRV8432DKDEVM_RevA.zip) but I am not able to open these pcb files. I tried using Express PCB,Mentor Graphics PowerPCB, Proteus also.

In the PDFs folder there are pcb layout files(topcopper,bottom copper,silkscreen etc) but when I took printout of them they are going out of dimensions.I tried everything but printouts are not  coming in exact dimensions thats why I am not able to make the pcb. In the DRV8432DKDEVM_RevA-DrillDrawing.pdf it is written that the board size is 130 X 80mm but in other pdfs these dimensions are not coming.

Can you please provide me the pcb layout files (.jpeg preferred) so that I can directly take the printout of them and make the pcb.It will be very helpful for me if you provide me that.

Thanks and Regards,

Onkar Pardeshi