Part Number: TMS320C203
Other Parts Discussed in Thread: DRV8300, DRV8353
I’m reaching out to see if you could provide some technical/design support for a hybrid motor controller we’re developing for an outboard application. We’re in the early stages and looking for general guidance as we define the system.
As a starting point, the system will be based on an 80 V battery with an initial current target of ~50 A.
In particular, we’d appreciate any input on:
- Power stage / inverter selection
- Control approach for hybrid operation
- Device recommendations (SiC, GaN, etc.)
- Thermal and marine environment considerations
If you have any relevant reference designs or application notes, that would be very helpful as well.
Let me know if you’d be open to a quick call to discuss.