Part Number: DRV8323
Hi Team,
Could you please help to check the questions from customer as below? Thanks.
- When VREF is powered by 3.3V & no VM, enable is pulled to high, will DRV8323 turn on some pins? Is any leakage concern for this condition?
- When VREF is powered by 3.3V & no VM, enable is pulled to low, will DRV8323 turn on some pins internally? Is any leakage concern for this condition?
- When enable keeps low, is there power sequence requirement of VREF & VM ? Is yes, which one should power on first?
- Our application has an accident condition that is : VREF & VM & enable are on at the same time , INHA & INLB are pulled to high by controller, CAL (DRV8323 input pin) is also pulled to high accidentally by external circuit, we didn’t see damage on DRV8323, but this condition caused damage of peripheral circuit. Do you have any idea of the damage path?
- To mitigate the condition4, we would like to modify design to : VREF & enable on, VM is off, CAL will not be pulled high, but INHA & INLB will be high at this time because of the limitation of controller, any concern of this condition? Especially the risk caused by IO out of control under this condition.
Best regards,
Terry