Hello all,
I am currently working on a project that uses DRV8825 (http://www.ti.com/product/DRV8825). I would like to have the Eagle files for it if TI community have it. Otherwise, I can use HTSSOP PWP 28 footprint and build it from there. I noticed that in texas.lbr (Eagle library), there's a package named HTSSOP28PWP, I can see it as a package in the library but it is not "attach" to any device. So when I use the "Add" command in a schematic, I do not see the package listed on there. May I know how do I use the package so it can be converted into DRV8825?
If Eagle schematic for DRV8825 or any related chip is available, that will be great too.
Thanks!