Part Number: DRV8323R
Other Parts Discussed in Thread: DRV8323, LMR16006
Hi,
related to my last topic "DRV8323R gate fault", locked without answer.
We’re going on with prospections and tests on driver gate failure.
First, I’ve got one question: I saw in a post that service life of driver was 100 000 hours at 105°C.
Please, what is the frequency of the PWM for this specification?
Our system works at 30 kHz PWM frequency.
Voltage measures didn’t give any clue, all seem normal.
Current measures are difficult because we use very small Idrive.
Around 50% of time, the three top Mosfets conduct simultaneously, because the nominal behavior of our system is motor waiting in the same position with pretty low current to hold a force.
May be the use of the driver as we do it is not suitable?
Experiment in progress is using DRV8323 with 8kHz PWM frequency.
Our hypothesis is that working at the lowest frequency will extend service life, isn't it?
Issue is still there, thank you for advising us.
Best regards
Alex